I am the beginner of DM365_EVM, now I have established my software systeme, the DVSDK I use is DVSDK_3_10_00_19, the filesystem I use for DM365 is montavista linux(NFS filesysteme), now I can lance the linux in DM365, but when I try to use the demo encoderdecoder, there is an error
Error: Failed to detect video standard, video input connected? Error: Failed to create Ir Object Error: Failed to create video decoder: mpeg4dec
And further more, when I used only the decoder, there is this error
Error: Failed to create Ir Object
My question is 1)what is Ir Objet, how can I solve this problem?
2)I think I have already add MT9D131(My camera) support when I compiled the kernel linux, but why it can not be detected.
3)Is there any document which I can refer to.
Thank you very much.