This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Temporarily stop USB3.0 with software

Part Number: AM5728

Hi experts,

Is there a way to temporarily stop the AM5728 USB3.0 with software?

My customer has a USB connection with the following configuration:

USB2.0 uses a USB switch to switch the USB memory connection destination between AM5728 and CPU.
USB3.0 connects directly to AM5728 from a USB memory.

When using a USB 2.0 USB memory, you can switch between AM5728 and CPU without any problem. However, if you use a USB3.0 USB memory, even if you want to interact with the CPU, it will be forcibly connected to the AM5728's USB3.0 port.

So they want to force the AM5728's USB3.0 to be disabled.

Best regards,
Sasaki