I had run the debug program and the results that are show in the display
are not logic, 90% and a Heart rate of 200 normally.
I would like to know what can I do to fix it?
Or where can I make test of the signal in order to know the problem?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I had run the debug program and the results that are show in the display
are not logic, 90% and a Heart rate of 200 normally.
I would like to know what can I do to fix it?
Or where can I make test of the signal in order to know the problem?
Thanks
Can you provide more information on your issue? What hardware / software are you using?
The software I use to run the debug program is: EVM5505 CCStudio V3.3
The hardware is:
DSP : TMS320C5505 EVM with the analog Front end Module for C5505 Medical Development kit.
The PC has Windows XP, Pentium Dual Core with 896 MB of RAM, 2.5Ghz.
If you need more information tell me...