This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Qt Creator OMAP-L138 and Building DVSDK qtopia example widgets

Other Parts Discussed in Thread: OMAP-L138

Hello I have Qt Creator 2.1.0 based on Qt 4.7.1 (32 bit) running under Ubuntu 10.04.LTS with a target of a OMAP-L138 evaluation board.

I went in to Qt Creator Tools-->Options-->Qt4 and manually added a Version named Qt Embedded and pointed the qmake location to be

/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/linux-devkit/bin/qmake

Two things I note

1 there is no mkspec:

0552.Qt-creaitor1.pdf

2 there is never a Auto-detected Qt in PATH

3 there is a message at the bottom of  Qt Creator Tools-->Options-->Qt4

Qt version is not properly installed, please run make install.

Where does it want me to run make install from ? Or ??

How do I get a mkspec into the above.

How do I get the Auto-detected Qt in PATH to show up, or is it necessary.

If I shut down Qt-Creator and restart from the command line ie

user@user-desktopUbuntuLTS:~/QtSDK/QtCreator/bin$ ./qtcreator

the previousely manually added Version named Qt Embedded is no longer there.

My goal is to be able to compile some of the supplied Qt widgets in the DVSDK using Qt-Creator and run them on the OMAP-L138 evaluation board touch screen.

Any help or point me to links that may be able to help would be appreciated...

I am a nubee to Qt-Creaitor, and may be trying to do this all wrong?

I did look at

http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/p/85114/391330.aspx#391330

and it seemed Anton got most of the locations / tools etc. found out of the box... I do not see this?

Please advise any links / advice / examples you can for my issues... Thanks