Has anyone was able to get GStreamer to work with arago? and if you did can I see the filesystem or tell me how you did it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Has anyone was able to get GStreamer to work with arago? and if you did can I see the filesystem or tell me how you did it?
Here an example (jresize and jpeg encoding) based on dvsdk4.02 on dm365
gst-launch v4l2src always-copy=FALSE ! queue ! videorate ! 'video/x
-raw-yuv,width=720,height=480,format=(fourcc)UYVY,framerate=(fraction)10/1' ! TI
VidResize contiguousInputFrame=TRUE ! 'video/x-raw-yuv,width=320,height=240,form
at=(fourcc)UYVY' ! TIImgenc1 resolution=320x240 iColorSpace=UYVY oColorSpace=YU
V420P qValue=75 engineName=codecServer codecName=jpegenc numOutputBufs=3 ! tcp
serversink port=10000
I would like to do the same integrating it in arago and OE, but I have to do it.
I have also a h264 pipeline and streaming working.
I have not yet clearly understood anyway if gstreamer in dm365 is recommended or it is better to move to dmai layer.
The goal is h264 encoding and udp streaming
Thank Raffaele, were you able to get it working with a camera sensor? I seen this done with montavista, but I havent seen anyone able to get a sensor working and able to see on the web browser, and this chip been in the market for almost 5 years I think.I seen the DM355 is becoming obsolete before it became an end product. :( I hope is not going to be the same with the dm365