Other Parts Discussed in Thread: AM4378
Hi,
We are switching our custom board design with AM4378 to AM6252 SoC. We used to have just MAIN domain with AM4378. However AM62xx series comes with 3 different domains (MAIN, MCU and WKUP). What are the use case differences between MAIN, MCU and WKUP domains? What kind of differences may occur using the communication interfaces of these different domains. Such as, which UART interface should I use for debugging purpose? I need an extra UART interface besides the MAIN UARTs , should I use MCU UART or WKUP UART? Also, the same applies for the SPI interace.
Thanks,
Best Regards.