Part Number: AM3358
Hello Champs,
Customer followed the steps according to below link.
6.1.9
https://software-dl.ti.com/processor-sdk-linux/esd/AM335X/08_02_00_24/exports/docs/linux/How_to_Guides/Host/How_to_Setup_Ubuntu_1404_Network_Boot.html
But the BBB board failed in network boot.
Below is the log.
Welcome to minicom 2.8
OPTIONS: I18n
Port /dev/ttyUSB0, 10:12:30
Press CTRL-A Z for help on special keys
CCCCCCCC
U-Boot SPL 2021.01-g44a87e3ab8 (May 14 2022 - 22:32:40 +0000)
Trying to boot from USB eth
eth0: eth_cpsw, eth1: usb_ether
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC de:ad:be:ef:00:01
HOST MAC de:ad:be:ef:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
USB RNDIS network up!
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
BOOTP broadcast 12
BOOTP broadcast 13
BOOTP broadcast 14
BOOTP broadcast 15
BOOTP broadcast 16
BOOTP broadcast 17
Retry time exceeded; starting again
Problem booting with BOOTP
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
CCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCC
How to resolve it?
Thanks.
Rgds
Shine