Part Number: AM625
Hi Experts,
I have a question about AM62x processors.
I have seen that they have two ethernet PHY and the EVM kit has two rj45 connectors. but in the datasheet, It seems that both rj45 are connected to an internal Ethernet switch.
The question is, has the processor two independent LAN? or there is only one MAC address/one IP address?
I need to have two distinct LAN (one for gigabit communication with a particular system and another connected to another LAN, both LAN must be gigabit and they must be separated, not connected through a switch.
Thank you.
Regards,
Archie A.