This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Powering the USB and RTC Module on TMS320VC5509A/07/06/03 devices.



If I don`t want to use the USB and RTC module on the C5509A/07/06/03 devices , would it matter if I did not power their corresponding power pins USBVdd and RDVdd RCVdd? Will this affect the proper functioning of other modules.
Answer: Even if the RTC or USB module are not used, both modules have to be powered. For RTC and USB module, RDVdd RCVdd and USBVdd pins have to be connected to their corresponding power supplies and ground pins.  C5509A/07/06/03 data manuals have the recommended connections.