This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PRUSS Maximum Rate



What is the maximum rate at which I can run PRUSS I have to do T1 framing which is 1.5Mbps can I do that using Pruss??

 

Thanks 

 

  • Roh@n T@bish

    Roh@n T@bish said:
    What is the maximum rate at which I can run PRUSS

    PRUSS core frequency can run at (1/2) SYSCLK1 Frequency. Please refer to the respective System Reference Guide for clocking details / defaults.