Hi Team,
I use the TMDXEVM6678LE Rev.3B to test our algorithm. I find that when I use evmc6678l.gel to initialize the board, the time spend on the algorithm is 66ms, while when I use the function platform_init from ti.platform.evm6678l.ae66 to initialize the board, the time will be 97ms. After analysis, I find that when six cores manipulate the DDR3 at the same time, evmc6678l.gel initialized board work much better than platform_init from ti.platform.evm6678l.ae66. So whats the differences between the gel and the platform_init from ti.platform.evm6678l.ae66.
Best Regards
James Man
TI Customer Support Center