This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Overread VUI by 196 bits



Hi ALL:

            I have tried use VLC/Mplayer to play the H264 streaming from DM365, and I found that x264 codec will popup warning message as:

[H264 @ 0xab0940]Overread VUI by 196 bits

            Any one who can help explain this?

            is there any method can avoid this warning message?

            Thanks in advance!

  • Tracy,

    The stream generated by DM36x is 100% compliant to H,264 spec, we check it using MTS4EA analyzers. Ideally, decoder should not throw any error. Can you send us a sample stream ? In case you want to disable VUI generation, you can set enableVUIparams = 0.

    regards

    Yashwant