This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Silencing printouts in TIDL

Part Number: TDA4VM

Hi, 

What is the simplest way to build 'libtidl_tfl_delegate.so' and 'libvx_tidl_rt.so' in the SDK such that all of these printouts are silenced when I run inference in a c++ example app?

APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
450320.328599 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
450320.328641 s: VX_ZONE_INIT:Enabled
450320.328755 s: VX_ZONE_ERROR:Enabled
450320.328794 s: VX_ZONE_WARNING:Enabled
450320.329211 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
450320.329334 s: VX_ZONE_INIT:[tivxHostInitLocal:86] Initialization Done for HOST !!!
450320.585234 s: VX_ZONE_INIT:[tivxHostDeInitLocal:100] De-Initialization Done for HOST !!!
450320.589728 s: VX_ZONE_INIT:[tivxDeInitLocal:193] De-Initialization Done !!!
APP: Deinit ... !!!
REMOTE_SERVICE: Deinit ... !!!
REMOTE_SERVICE: Deinit ... Done !!!
IPC: Deinit ... !!!
IPC: DeInit ... Done !!!
MEM: Deinit ... !!!
MEM: Alloc's: 9 alloc's of 5894245 bytes
MEM: Free's : 9 free's of 5894245 bytes
MEM: Open's : 0 allocs of 0 bytes
MEM: Deinit ... Done !!!
APP: Deinit ... Done !!