Part Number: SK-AM62
Hello,
I'm trying to load rootfs on the eMCC of the SK-AM62 evaluation board.
I have built u-boot to use USB DFU and I can start DFU on the u-boot console ("dfu 0 mmc 0").
When I try to load the rootfs with the following command:
sudo dfu-util -a rootfs -D tisdk-base-image-am62xx-evm.ext4
this fails and the following log is displayed in the u-boot console:
################################################################Request would exceed designated area!
Any idea of the issue here ?
I suspect something is wrong in the bootloader config for this board...
Thanks,
Joel