Part Number: 66AK2E05
How to run TSIP project from TI-RTOS SDK on DSP core of K2E processor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: 66AK2E05
How to run TSIP project from TI-RTOS SDK on DSP core of K2E processor?
To run the TSIP (T1 / E1) Example project for K2E devices make sure the pre-requisites are done.
Now Import the CCS project into CCS and go on

//Sample.c
void tsipConfig (tsipSizeInfo_t *sizeCfg, tsipConfig_t *cfg)
{
/* Provide size information for TSIP */
sizeCfg->maxChannels = TSIP_MAX_TIMESLOTS;
sizeCfg->subFrameSize = 8;
sizeCfg->wordSize = 8;
sizeCfg->validParams = TSIP_SIZE_INFO_VALIDPARAMS_NUM_PORTS;
sizeCfg->numPorts = NUM_USED_TSIP_PORTS;
/* Global configuration */
cfg->testMode = TRUE;
cfg->testModeSelect = CSL_TSIP_TESTMODE_DATA_LOOPBACK;
cfg->clkRedund = CSL_TSIP_CLKD_REDUN;
cfg->endian = CSL_TSIP_ENDIAN_LITTLE;
cfg->priority = CSL_TSIP_PRI_0;
cfg->maxPriority = CSL_TSIP_PRI_0;
cfg->sizeCfg = sizeCfg;
cfg->maxPhase = 10;
cfg->subFrameCallout=NULL;
cfg->cxt=NULL;
/* Transmit configuration */
cfg->tx.channel = deviceWhoAmI();
cfg->tx.frameSize = CSL_TSIP_FRAMESIZE_128;
cfg->tx.tsPerFrame = 256;
cfg->tx.clkSrc = CSL_TSIP_CLKSRC_A;
cfg->tx.dataDelay = 1;
cfg->tx.bdxDelay = CSL_TSIP_DLY_CTRL_DISABLE;
cfg->tx.idleDrive = CSL_TSIP_XMTDIS_HIGHIMP;
cfg->tx.fsyncPol = CSL_TSIP_FSYNCP_ALOW;
cfg->tx.fsyncClkPol = CSL_TSIP_CLKP_RISING;
cfg->tx.clkPol = CSL_TSIP_CLKP_RISING;
cfg->tx.dataRate = CSL_TSIP_DATARATE_16M;
cfg->tx.clkMode = CSL_TSIP_CLKM_SGL;
cfg->tx.superFrameInt = CSL_TSIP_INT_ACK;
cfg->tx.frameInt = CSL_TSIP_INT_ACK;
cfg->tx.frameIntDelay = 0;
/* Receive configuration */
cfg->rx.channel = deviceWhoAmI();
cfg->rx.frameSize = CSL_TSIP_FRAMESIZE_128;
cfg->rx.tsPerFrame = 256;
cfg->rx.clkSrc = CSL_TSIP_CLKSRC_A;
cfg->rx.dataDelay = 1;
cfg->rx.bdxDelay = CSL_TSIP_DLY_CTRL_DISABLE;
cfg->rx.fsyncPol = CSL_TSIP_FSYNCP_ALOW;
cfg->rx.fsyncClkPol = CSL_TSIP_CLKP_RISING;
cfg->rx.clkPol = CSL_TSIP_CLKP_FALLING;
cfg->rx.dataRate = CSL_TSIP_DATARATE_16M;
cfg->rx.clkMode = CSL_TSIP_CLKM_SGL;
cfg->rx.superFrameInt = CSL_TSIP_INT_ACK;
cfg->rx.frameInt = CSL_TSIP_INT_ACK;
cfg->rx.frameIntDelay = 0;
}[C66xx_0] ************************************************** ******* TSIP Example Start *********************** ************************************************** TSIP port 0 is powered up TSIP driver instance successfully initialized TSIP port instance successfully initialized TSIP port 0 super frame interrupt is registered Initialize application buffers before TSIP-APP transfer Enabling TSIP timeslot TX 0 RX 0... TSIP timeslot TX 0 RX 0 successfully enabled TSIP data transfer...
Thanks & Regards,
Rajarajan U