Part Number: TDA4VM
Hi,
I would like to achieve a precise scaling in MSC (1/1.7778)x . Is it possible achieve precise scaling in MSC?
Regards,
Dinesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hi,
I would like to achieve a precise scaling in MSC (1/1.7778)x . Is it possible achieve precise scaling in MSC?
Regards,
Dinesh
1) I assume this is by considering 4096 as the entire frame width. But the same can be done for my ROI 2, let's say 1050 is my ROI of the input 1920. Your example should still be valid right?
2) Along with 1) will i be able to create 1x scaling for ROI 1 too.
Scaling factor is an user input parameter for MSC and you can vary the I/O image sizes independently from the scale factor.
For example, you may set your scale factor to 7282, input image width to 1920 and output width to 1080.
Hi, We tried scaling we are able to achieve 1 input and one 1.77778x output but we aren't able to achieve the second output from the same input that is 1x cropping. Is it like the 1 input 5 output works only on pyramid generation? and wont work for integer scaling?
Sounds Good, Is there a calculation methodology given for coefficient generation with respect to desired scaling ratios?.