Other Parts Discussed in Thread: TMS320VC5505
Hi all,
I have one question to ask. I have c5505evm on which it has 256Kbit spi eeprom to hold user code. Can I use 1 Mbit(24 bit serial) spi eeprom with C55? Is it compatible with tms320C55 device? If not so, what should I do with code size larger than 32KB with C5505?
Because I have read "Using the TMS320VC5505/04 Bootloader" application report and it says "The device uses 2 bytes (16 bits) for internal addressing (up to 64kB)."