I have tried very combination possible biut alway get the same result.
In the build property i have used large,small and none with the checkbox for large checked and unchecked.
I have combined that with Generic 5505, Generic 5505+ and Custom 5505.
Using rst55p.h as run time libs and the ezdsp usb stick.
I get this error.
fatal error: file "C:/Program Files/Texas Instruments/CCSv4/tools/compiler/c5500/lib/rts55p.lib<boot.obj>" specifies machine "TI C55x+", which is not compatible with machine "TI C55x" specified in a previous file or on the command line Thanks Martin