This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timers

What is the correct lib and c5505 for timers?

The build says "Small", lib is rts55p and device is generic 5505.

fatal error: file "C:/Program Files/Texas

Instruments/CCSv4/tools/compiler/c5500/lib/rts55p.lib<boot.obj>" specifies

small memory model, which is not compatible with large memory model

specified in a previous file or on the command line

================================================================================

A.1.02 Runtime Support Libraries

================================================================================

The runtime libraries for C55x+ are named "rts55p" instead of "rts55." For

example, the small model library is rts55p.lib. The byte mode libraries append

"b" to the usual names. Only Large and Huge Memory Models are supported for byte

 

Thanks

Martin