Part Number: TDA4VM
I have a set of TDA4VM board (E3 common board, E8 SOM board) can't boot up with PSDK8.2.
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')

With same common board work with E7 SOM board can boot up with same card as below:
U-Boot 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000)
SoC: J721E SR1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM: 4 GiB
not found for dev hbmc-mux
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
Replace the sysfw with a older one (From a old psdk6.x), can also boot up E8 SOM, but there is some error when driver initialize.
U-Boot 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000)
SoC: J721E SR2.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
DRAM: 4 GiB
not found for dev hbmc-mux
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
From the message, E8 board is SR2.0 SOC, how to make the E8 SOM board work with latest PSDK?