Starting to learn how to program for the USB Stick, starting with the TMS320 DSB/BIOS v5.40 User's Guide - spru423g, section 2.1.
Unable to build a project due to linkage failure - Unable to determine the cause of the linkage failure.
Build Failure - Project hellobias5
Project entered as defined in TMS320 DSP/BIOS v5.40 User's Guide section 2.1 except with
following selections:
Project Type: C5500 instead of C6000
Device Varient: TMS320C55XX instead of Generic 64x+ Device
Runtime Support Library: rts55h.lib
Used TI Simulator: C55x+ CPU Cycle Accurate Simulator
**** Build of configuration Debug for project hellobias5 ****
C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake -k all
'Building file: ../hellobias5.tcf'
'Invoking: TConf Script Compiler'
"C:/Program Files/Texas Instruments/xdctools_3_15_03_67/tconf" -b -Dconfig.importPath="C:/Program
Files/Texas Instruments/bios_5_40_03_23/packages"; "../hellobias5.tcf"
'Finished building: ../hellobias5.tcf'
' '
'Building file: ../hellobias5.c'
'Invoking: C5500 Compiler'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c5500/bin/cl55" -v5505 -g
--include_path="C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c5500/include"
--include_path="F:/ez-dsp Work Folder/hellobias5/Debug" --include_path="C:/Program Files/Texas
Instruments/bios_5_40_03_23/packages/ti/bios/include" --include_path="C:/Program Files/Texas
Instruments/bios_5_40_03_23/packages/ti/rtdx/include/c5500" --diag_warning=225 --sat_reassoc=off
--ptrdiff_size=32 --fp_reassoc=off --memory_model=huge --asm_source=mnemonic --preproc_with_compile
--preproc_dependency="hellobias5.pp" "../hellobias5.c"
'Finished building: ../hellobias5.c'
' '
'Building file: hellobias5cfg.s??'
'Invoking: C5500 Compiler'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c5500/bin/cl55" -v5505 -g
--include_path="C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c5500/include"
--include_path="F:/ez-dsp Work Folder/hellobias5/Debug" --include_path="C:/Program Files/Texas
Instruments/bios_5_40_03_23/packages/ti/bios/include" --include_path="C:/Program Files/Texas
Instruments/bios_5_40_03_23/packages/ti/rtdx/include/c5500" --diag_warning=225 --sat_reassoc=off
--ptrdiff_size=32 --fp_reassoc=off --memory_model=huge --asm_source=mnemonic --preproc_with_compile
--preproc_dependency="hellobias5cfg.pp" ""
Command-line error: missing source file name
1 fatal error detected in this compilation.
Compilation terminated.
>> Compilation failure
C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: *** [hellobias5cfg.obj] Error 1
'Building file: hellobias5cfg_c.c'
'Invoking: C5500 Compiler'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c5500/bin/cl55" -v5505 -g
--include_path="C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c5500/include"
--include_path="F:/ez-dsp Work Folder/hellobias5/Debug" --include_path="C:/Program Files/Texas
Instruments/bios_5_40_03_23/packages/ti/bios/include" --include_path="C:/Program Files/Texas
Instruments/bios_5_40_03_23/packages/ti/rtdx/include/c5500" --diag_warning=225 --sat_reassoc=off
--ptrdiff_size=32 --fp_reassoc=off --memory_model=huge --asm_source=mnemonic --preproc_with_compile
--preproc_dependency="hellobias5cfg_c.pp" ""
Command-line error: missing source file name
1 fatal error detected in this compilation.
Compilation terminated.
>> Compilation failure
C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: *** [hellobias5cfg_c.obj] Error 1
C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors.
Build complete for project hellobias5
Problem Description:
Severity and Description Resource Location
Linking failed. hellobias5 Unknown
Debug Folder Files:
hellobias5cfg.h, hellobias5cfg_c.c, hellobias5cfg.s55, hellobias5obj - [C5500be],
ccsObjs.opt, hellobias5.cdb, hellobias5.pp, hellobias5cfg.cmd, hellobias5cfg.h55
makefile, objects.mk, sources.mk, subdir.mk
Source Files:
hellobias5.c, hellobias5cfg.h, log.h, std.h, main
Target Configuration File: C55x+ CPU Cycle Accurate Simulator
ezdspsim.ccxml [Active]
hellobias5.tcf