hi , TI experts:
We are working on several yuv422 8bit cameras connect to CSIRX via max9295a/max96712 deserializes,the tda4 can not receive camera data, and the deserializer output signals MIPI clk, and data are all good. The SDK version is ti-processor-SDK-RTOS-j721e-EVM-08_01_00_11. The test program used is vision_apps\apps\basic_demos\app_single_cam. The sensor configuration is as follows:
and the Input to Stream FSM states is PROT_WAIT_CTRL , is it the tda4 not receice the data of deserializer?
below is the data lane wave of deserializer:
and our max96712, Install virtual channel 0 in max96712 video pipes 0,
Install virtual channel 1 in max96712 video pipes 1,
Install virtual channel 2 in max96712 video pipes 2,
Install virtual channel 3 in max96712 video pipes 3,
and i have moved our deserializer complete initialization configuration and streamon configuration to streamon callback.
but when i read value of register 0x045900E8(use cis1 via select (cam id 4-7) ), it is 0x02, i don't know DPHY PLL CLK is locked or not locked?
i don't konw whether the 0other parts of tda4 need to config?
thanks!!