This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Audio Passthrought code for ezDSP



Hi,

I need simple audio passthrough code for ezDSP. I tried to alter aic3204 sample code that comes with CCS v4 but was not able to get it done correctly. Can anyone help on this.

Thanks,

Abhishek Seth 

  • Hi Abhishek,

    We have provided Audio Filtering code for the EZDSP at the following site, the link for the code is towards the bottom of the page.

    http://code.google.com/p/c5505-ezdsp/

    Here is a description of what the code does:

    This program takes audio input through I2S interface, then send back to I2S again.
    Between intput and output:
    FIR filter for 10 seconds (LED tunred on)
    No filter for 10 seconds (LED turned off)

    1) I2S interface
    - Audio Codec: ADS3204 (Master/Slave)
    - C5505 (Slave/Master)
    - Sampling rate: 48KHz

    2) Data
    - Use Pingpong buffer  (two L inputs, two R inputs, two L outs, two R outs): total 8 buffers
    - Buffer size: 48*2 words (16bit)

    3) Filter
    - FIR filter
    - Fc = 2KHz
    - -80dB@ 10KHz
    - -1dB@1KHz

    Best regards, Vishal

  • Hi Vishal,

    Thanks for your reply. I downloaded the passthrough code and it is working fine. I want to change the ADC and DAC sampling rates from 48 KHz to 192 KHz. How to do this ?

    Thanks,

    Abhishek Seth.

  • Hi Abhishek Seth,

     

    Please get the datasheet of the AIC3204 form this link: http://focus.ti.com/lit/ds/symlink/tlv320aic3204.pdf  You should be able to see registers that you need to modify for sampling rate change.

    In the audio demo code, "aic_test_i2c.asm" file has the configuraitons for the audio codec, for example:

            AC1 = #1
            AR1 = #0x1
            call i2c_WriteData8

    The first line is register address. The Second line is a value you want to write to the register. Basically, you are writing "1" to the register "0x01".

     

    Thanks,

    Peter Chung

     

  • i'm getting a warning when i build.

    Severity and Description    Path    Resource    Location    Creation Time    Id
    entry-point symbol other than "_c_int00" specified:  "reset_isr"        EZDSP_AudioFilter    line 0    1258497226487    3

    i'm new at evaluating TI dsp, so i'm not sure if this is a good or a bad thing. any help?

    -drb.

     

  • Hi David,

    You are OK with this warning. By default, CCS is expecting the _c_int00 in the C Run Time Support Library (RTS) as the extry point. This example uses the reset_isr as the entry point instead. That is why the CCS gives the warning.

    Ming