Part Number: AM3358
Hello,
I am facing below error while building kernel from local workspace. If I do not have workspace then I don't see any error. Can you help me on resolving this? I need to have workspace since I am working on kernel related changes. I am using dunfell branch of meta-ti.
Loading cache: 100% |#########################################################################################################| Time: 0:00:00Loaded 4480 entries from dependency cache.WARNING: /home/aws-fsp-build/rax-workspace/yocto/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_5.10.bb: Exception during build_dependencies for do_configureWARNING: /home/aws-fsp-build/rax-workspace/yocto/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_5.10.bb: Error during finalise of /home/aws-fsp-build/rax-workspace/yocto/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_5.10.bbERROR: ExpansionError during parsing /home/aws-fsp-build/rax-workspace/yocto/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_5.10.bbTraceback (most recent call last): File "Var <KERNEL_LOCALVERSION>", line 1, in <module>bb.data_smart.ExpansionError: Failure expanding variable KERNEL_LOCALVERSION, expression was -g${@d.getVar('SRCPV', True).split('+')[1]} which triggered exception IndexError: list index out of range
WARNING: /home/aws-fsp-build/rax-workspace/yocto/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_5.4.bb: Cooker received SIGTERM, shutting down...WARNING: /home/aws-fsp-build/rax-workspace/yocto/meta-carrier/recipes-kernel/linux/linux-ti-staging_4.19.bb: Cooker received SIGTERM, shutting down...WARNING: /home/aws-fsp-build/rax-workspace/yocto/meta-carrier/recipes-kernel/mstp-mod/mstp-mod.bb: Cooker received SIGTERM, shutting down...
Summary: There were 5 WARNING messages shown.Summary: There was 1 ERROR message shown, returning a non-zero exit code.
Regards,
Raxesh