Part Number: TDA2SX
Other Parts Discussed in Thread: TDA2
Hi team,
Here's an issue from the customer may need your help:
The IPv6 address protocol is used in TDA2 to send UDP message data. By creating a SOCKet, but failed, the code is as follows:
static char src[] = "fd11::100";
static char dst[] = "fd11::200";
void main_Tx()
{
int udp6_socket, ret, ttl, on, addr_len;
struct sockaddr_in6 saddr;
struct sockaddr_in6 daddr;
char buffer[] = "Hello World6";
Vps_printf(" DanS-----Network: start IPv6 interface main\n");
if ((inet_pton(AF_INET6, (char *)&src[0], &saddr.sin6_addr)) != 1)
{
Vps_printf("invalid ipv6 addr \r\n");
return ;
}
if ((inet_pton(AF_INET6, (char *)&dst[0], &daddr.sin6_addr)) != 1)
{
Vps_printf("invalid ipv6 addr \r\n");
return ;
}
addr_len = sizeof(struct sockaddr_in6);
saddr.sin6_family = AF_INET6;
saddr.sin6_port = htons(30000);
daddr.sin6_family = AF_INET6;
daddr.sin6_port = htons(40000);
udp6_socket = socket(AF_INET6, SOCK_DGRAM, IPPROTO_UDP);
if (udp6_socket == -1)
{
Vps_printf("create udp6_socket fail\r\n");//the codes are run and printed here
Vps_printf("failed socket create (%d)\n",fdError());
return;
}
if (bind(udp6_socket, (struct sockaddr *)&saddr, addr_len))
{
Vps_printf("udp6 bind addr fail, err : %d\r\n", 0);
if( udp6_socket != (-1) )
fdClose( udp6_socket );
Vps_printf("\n== End Timeout Test ==\n\n");
//close(udp6_socket);
return;
}
/* transmit */
ret = sendto(udp6_socket, &buffer[0], sizeof(buffer), 0, (struct sockaddr *)&daddr, addr_len);
if (ret > 0)
{
Vps_printf("udp6 send %d bytes success \r\n", ret);
}
fdClose( udp6_socket );
//close(udp6_socket);
return;
}
The error is reported in yellow section.
a. The NDK_enable_IPv6 switch for the corresponding usecase has been turned on in TDA2.
b. What else needs to be modified for IPv6 to function properly? Could you help give an example?
Could you help check this case? Thanks.
Best Regards,
Cherry