Hello all,
I run camera app of vision_apps on TDA4VM-EVM without camera but it didn't read test raw file and pass the test without processing.
What is my problem?
Below are my input command and messages.
root@j7-evm:/opt/vision_apps# ./vx_app_single_cam.out --cfg app_single_cam.cfg --test APP: Init ... !!! MEM: Init ... !!! MEM: Initialized DMA HEAP (fd=4) !!! MEM: Init ... Done !!! IPC: Init ... !!! IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! 216956.151198 s: GTC Frequency = 200 MHz APP: Init ... Done !!! 216956.155140 s: VX_ZONE_INIT:Enabled 216956.155153 s: VX_ZONE_ERROR:Enabled 216956.155197 s: VX_ZONE_WARNING:Enabled 216956.157479 s: VX_ZONE_INIT:[tivxInit:71] Initialization Done !!! 216956.157701 s: VX_ZONE_INIT:[tivxHostInit:48] Initialization Done for HOST !!! sensor_selection = [0] ldc_enable = [0] num_frames_to_run = [1000000000] is_interactive = [1] IttCtrl_registerHandler: command echo registered at location 0 IttCtrl_registerHandler: command iss_read_2a_params registered at location 1 IttCtrl_registerHandler: command iss_write_2a_params registered at location 2 IttCtrl_registerHandler: command iss_raw_save registered at location 3 IttCtrl_registerHandler: command iss_yuv_save registered at location 4 IttCtrl_registerHandler: command iss_read_sensor_reg registered at location 5 IttCtrl_registerHandler: command iss_write_sensor_reg registered at location 6 IttCtrl_registerHandler: command dev_ctrl registered at location 7 IttCtrl_registerHandler: command iss_send_dcc_file registered at location 8 NETWORK: Opened at IP Addr = ***.***.***.***, socket port=5000!!! 216956.160427 s: ISS: Enumerating sensors ... !!! 216956.161008 s: ISS: ERROR: Enumerating sensors failed !!! Invalid sensor selection 255 Error : app_init returned 0xffffffff 216956.161253 s: ISS: De-initializing sensor [Noname] ... !!! 216956.161366 s: ISS: De-initializing sensor [Noname] ... Done !!! TEST PASSED 216956.161390 s: VX_ZONE_INIT:[tivxHostDeInit:56] De-Initialization Done for HOST !!! 216956.165714 s: VX_ZONE_INIT:[tivxDeInit:111] De-Initialization Done !!! APP: Deinit ... !!! REMOTE_SERVICE: Deinit ... !!! REMOTE_SERVICE: Deinit ... Done !!! IPC: Deinit ... !!! IPC: DeInit ... Done !!! MEM: Deinit ... !!! MEM: Alloc's: 0 alloc's of 0 bytes MEM: Free's : 0 free's of 0 bytes MEM: Open's : 0 allocs of 0 bytes MEM: Deinit ... Done !!! APP: Deinit ... Done !!!
Could you help me and point out the reason?
Best regards,
Okabe