This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4372: Build-up PCB and multi-layer through-hole PCB

Guru 10245 points

Part Number: AM4372
Other Parts Discussed in Thread: AM4376

Hi Support Team,

AM4372 is used and mounted on a build-up PCB, are there any restrictions?
If so, what are the reasons?

Also, is it possible to mount AM4376 on a multi-layer through-hole PCB?

For your information, our customer is using AM4372 and AM4376.

Kanae

  •  ?Hello Kanae, 

    Thank you for the query.

    Could you please help me understand your query

    AM4372 is used and mounted on a build-up PCB, are there any restrictions?

    Please help me understand which  board are you referring to

    Also, is it possible to mount AM4376 on a multi-layer through-hole PCB?

    I need you help to understand the question since AM4376 is a BGA package device.

    Regards,

    Sreenivasa

  • Hi Sreenivasa,.

    Thank you for your reply.

    Sreenivasa:
    Please help me understand which board are you referring to"

    Please see the following reference site for a general description of the "build-up board (PCB)"
    you are using that implements the AM4372 on your custom board.

    www.atc-kr.com/.../build-up-pcb-printed-circuit-board.html

    The background to our customer's question is that our customer is considering
    whether the build-up board on which the AM4372 is currently mounted can be changed
    to a multilayer through-hole board in order to reduce costs.
    Therefore, they want to confirm if it is possible to mount AM4372 on a multilayer through-hole board.

    Sreenivasa:
    "I need you help to understand the question since AM4376 is a BGA package device."

    Similar to the above question about AM4376, our customer just wants to confirm
    whether AM4376 can be mounted on a multilayer through-hole board or not.
    What exactly do you need help with?

    Our customer wants to confirm the answer by June 29th, so please let us know
    when you will respond if it is difficult to respond as soon as possible.

    Best regards,
    Kanae

  • Hello Kanae, 

    Please refer below

    What exactly do you need help with?

    Also, is it possible to mount AM4376 on a multi-layer through-hole PCB?

    I was trying to understand the above question. BGA getting mounted on the  through-hole PCB

    Based on the inputs above, my quick thought is customer can consider a SOM and a carrier bboard option to reduce the 

    Regards,

    Sreenivasa

  • Hi Sreenivasa,.

    Thank you for your prompt reply.

    Sreenivasa:
    "Based on the inputs above, my quick thought is customer can consider a SOM and a carrier bboard option to reduce the ..."

    The sentence is broken, what do you mean by "reduce"?
    The customer is looking to reduce costs.

    Also, in your reply you state, "customer can consider a SOM and a carrier board option", what exactly is the option?
    Does this answer mean that a multi-layer through-hole PCB cannot be used?

    The customer wants to confirm a clear answer by June 29th, so please let us know
    when you will respond if it is difficult to respond as soon as possible.


    Best regards,
    Kanae

  • Hello Kanae,

    Please refer below 

    Based on the inputs above, my quick thought is customer can consider a SOM (System on module) and a carrier board option to reduce the board size.

    The customer is looking to reduce costs.

    This depends on the overall board size and layer count. The SOM will have larger layer count and the carrier will have smaller count.

    The customer wants to confirm a clear answer by June 29th, so please let us know when you will respond if it is difficult to respond as soon as possible.

    Please note that we can provide answers related to the EVM and we do not have any suggestion regarding the PCB fab process that we do not follow. 

    regards,

    Sreenivasa

     

     

  • Hi Sreenivasa,

    Thank you for your support.
    I will share this with our customer.

    Best regards,
    Kanae

  • Hello Kanae,

    Noted and thank you.

    Regards,

    Sreenivasa