This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem with respect to the CVBS display



Hello,

We are facing some problem with respect to the CVBS display, on a 3503 based board with Android 2.2 kernel from rowboat-froyo running on it.

I have attached the two pictures taken from CVBS as well as VGA display.

In case of CVBS display the place where two different colors are adjacent to each other, the edges are not smooth. As from the picture, it appears as if the Red color has got spilled on to the Yellow one at the edges(In between two Yellow elements).
This is just an example I have shown in pictures, though it happens with other colors and at other places in UI as well.

Can somebody give some Idea, as to what might be the problem area?

I have verified the venc registers as per the TRM.

I also captured the screen image(from RAM) from DDMS to check if the composition is having any issues, even that is fine.

regards
-Nitin