Hello all,
I would like to process RAW image(12b packed) files using HWA and ISP on TDA4VM.
I have tried to use `app_single_cam` but it has critical comment is "Supports only RAW 12b Unpacked format" in below code.
vx_int32 read_test_image_raw(char *raw_image_test_fname, tivx_raw_image raw_image, vx_uint32 test_mode) { char raw_image_fname[MAX_FNAME] = {0}; char failsafe_test_data_path[3] = "./"; char * test_data_path = app_get_test_file_path(); FILE * fp; vx_uint32 width, height, i; vx_imagepatch_addressing_t image_addr; vx_rectangle_t rect; vx_map_id map_id; void *data_ptr; vx_uint32 num_bytes_per_pixel = 2; /*Supports only RAW 12b Unpacked format*/ vx_uint32 num_bytes_read_from_file = 0; tivx_raw_image_format_t format; vx_uint32 imgaddr_width, imgaddr_height, imgaddr_stride;
How can I feed 12Bit packed RAW to VISS?
Is there way to convert 12bit packed RAW to unpacked RAW using HWA?
Best regards,