This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ITBOK Memory Test Issue

hi,

 I am using AM/DM 37xx Evalution Board .

I am trying to test Memory RAM using ITBOK.

my RAM starting Address is  0x80000000 and end address is 0x8FFFFFFF so number of Bytes is 0xFFFFFFF

For address bus test .

 

typedef volatile unsigned char REG_U8

addressMask = (nBytes/sizeof(REG_U8) - 1);

 pattern = (REG_U8) 0xAAAAAAAA;
 antipattern = (REG_U8) 0x55555555;

    
  printf("Running address bus test...");
  /* Write the default pattern at each of the power-of-two offsets. */
  for (offset = sizeof(REG_U8); (offset & addressMask) != 0; offset <<= 1) {
                      baseAddress[offset] = pattern;
   }

   /* Check for address bits stuck high. */
   testOffset = 0;
    baseAddress[testOffset] = antipattern;

    for (offset = sizeof(REG_U8); (offset & addressMask) != 0; offset <<= 1) {
        if (baseAddress[offset] != pattern) {
                        printf("SDRAM - Address Bus Test failed at 0x%x\n", offset);
                        printf("SDRAM - Check for address bits stuck high failed.\r\n");
                        p_test_status = test_status = FAILURE;
             }
      }

In my AM/DM 37x EVM Board , value of addressMask is  0xFFFFFFE 

so expression (offset & addressMask)   gives zero value at first time so never  goes inside  any of the for loop.

and address bus  testing is not perform .

help me ....