Part Number: AM625
The Boot Mode SW settings description in the User's Guide SPRUJ40 is rather confusing.
The section 2.5.16.2 vaguely states that
"The boot mode orientation has changed between E1 and E2. Please follow board silkscreen."
as well as
"Note: Actual Board Silkscreen May Appear Inverted in this Orientation. Follow Physical Switch Text"
To add to the possible confusion the UG shows
"Figure 2-7. Bootmode Switch Configuration for SD Boot (E1)"
I understand that board layout mistakes happen and are hard to fix. However, the lack of a clear description with corresponding figure in the User Guide is something that is hard to forgive.
In essence: The switches SW1 and SW2 are located and oriented (ON-OFF) as described in the UG. However, the bit assignment on each of the switches is mirrored with LSB on the left side and MSB on the right side. (that makes B15 adjacent to B0).
I hope this may help. If you just started with an EVM that never worked and you are not even sure if you flashed proper image on the uSD card then you may easily bur an hour or more in a trial/error mode.
What adds to it is the fact that pressing RESET button doesn't seem to re-read the SW configuration. One needs to power-cycle the EVM every time the configuration is changed.
"Follow board silkscreen?" = Look for tiny B0, B7, B8 and B16. Once you know what to look for it is obvious - but magnifying glass may be your friend.
Cheers - Martin