Part Number: TDA4VM
Hello,
We are working with PSDK-RTOS-J721E 07.01.00.11 and PSDK-QNX-J721E 07.01.01.00, and our QNX SDP version is 7.1. Due to the requirements of our project, we are constrained to these versions.
We are following the TI recommendation in E2E post at https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1011331/tda4vm-the-latest-version-of-qnx-bsp, which says that "...use that QNX BSP that is listed in the SDK release notes. If an earlier, or more recent QNX BSP is required, it may function as-is or may require minor modifications to get all the ... features functional".
The release notes for our version of PSDK-QNX at https://software-dl.ti.com/jacinto7/esd/processor-sdk-qnx-jacinto7/07_01_01_00/exports/docs/release_notes_07_01_01.html#qnx-dependency specify the following buildIDs of QNX packages.

When we attempted to install these packages from the QNX Software Center, the following versions were shown to us:
com.qnx.qnx710.bsp.ti_j721e_am752x_evm - BuildID 57
com.qnx.qnx710.target.screen.board.jacinto7 - BuildID 325
We were able to install and then downgrade the first component from buildID 57 to buildID 10.
But we are not able to locate/install the Screen board component with buildID 256. The QNX Software Center only allows the installation of Screen board component with buildID 325. We checked with our QNX support contact, and they confirmed that the Screen board component with buildID 256 is not available on their server.
How should we proceed further? Please advise.
Thanks and regards.