This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Process to load and run after a good build?

What are the steps to do after a good build?

Do I build for Release or Debug?

Thanks

Martin

  • Hi Martin,

    After building project, you can do the following steps:

    1. Build a new target configuration file for USB Stick, if it is not done yet.

    2. Debug Active Project using the target configuration file.

    3. Make final release and burn it into the EEPROM on USB Stick.

    Attached please find the detailed screen shots for those steps in PDF format. You may not have all the files needed, but you can get basic ideas. The hands-on project will release to public soon.

    The current build type is next to the project name [Active - Debug] means debug version [Active - Release] means release version.

    Ming

  • Thanks for the reply.

    Martin

  • Hi Ming,

    thanks for providing the pdf-file about the hands-on tutorial. You said the tutorial would be available to the public soon. Is there any news about this yet?

    Cheers and regards,

    Michael

  • Hi,

    I would also be interested in the tutorial, especially in the "C5505_USBKey_LED_Demo_CSL_1.0_CCS4.0_Full.zip" archive, as I am still having trouble with the execution from flash using the bootloader. Ist there any place where the example can be downloaded?

    Regards,

    Raphael