This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

kernel and filesystem not compatible,



I downloaded revision 37  source code for the DM365 and I downloaded revision 37 filesystem from arago.

the kernel image file goes under "2.6.32-rc2-davinci1"

I also I downloaded revision 38  source code for the DM365 and I downloaded revision 38 filesystem from arago.

the kernel image file goes under "2.6.32.17-davinci1"

if I use the the kernel from revision 38 with the filesystem from revision 37 it does not work it says module are not compatible,  even if I change on the kernel in the make file from 2.6.32.17-davinci1 to 2.6.32-rc2-davinci1, is they any other changes I have to make besides the make file or do know of any instructions of how to build the modules on the filesystem to be compatible with a different kernel version?

  • Except for the loadable modules, I usually find the kernel is more or less okay with any file system. I usually build the kernel first, then build the modules, eg.

    make modules ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi-

    Optionally you can install the modules on top of the existing FS (in /lib/modules) with

    make modules modules_install INSTALL_MOD_PATH=path_to_target_root ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi-

    I guess if you are loading modules automatically on boot, you need to install the modules. Otherwise, you should be able to just copy a specific .ko module out from the built kernel and load manually.

     

  • Thank you, that answers me that question, do you have any idea about the the GStreamer modules to be compatible with the kernel and filesystem I'm running

    http://e2e.ti.com/support/embedded/f/354/t/110943.aspx

  • Usually you compile your external modules in context of the kernel build. In your external module directory, something like this:

    make -C path_to_your_kernel SUBDIRS=path_to_your_other_kernel_code modules

    GStreamer looks to be tied up with bitbake. I don't know anything about GStreamer or bitbake.