This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

initrd ramdisk location



I'm using the DM6467 and I have a question about where to load the ramdisk.  The u-boot bootargs are set to "...root=/dev/ram0 rw initrd=0x85000000,16M mem=100M...".  So, I think I am putting the ramdisk toward the end of Linux memory.  It boots successfully.  I tried putting the ramdisk outside Linux memory at 0x8F000000, but it does not boot.  Error is "Kernel panic - not synching: VFS: Unable to mount root fs on unknown-block(1,0)".  Is the ramdisk required to go within the Linux memory?