Other Parts Discussed in Thread: OMAP3530, AM3517
Hi,
I am making a ubi.img and fastboot it to system partition of NAND,
1. Check mtdinfo by
$mtdinfo /dev/mtd/mtd4
mtd4
Name: jffs2-nand
Type: nand
Eraseblock size: 131072 bytes, 128.0 KiB
Amount of eraseblocks: 4036 (529006592 bytes, 504.5 MiB)
Minimum input/output unit size: 2048 bytes
Sub-page size: 512 bytes
OOB size: 64 bytes
Character device major/minor: 90:8
Bad blocks are allowed: true
Device is writable: true
2. Make ubi.img,
$ sudo mkfs.ubifs -r temp/ -m 2048 -e 131072 -c 4036 -o ubifs.img
$ ubinize -o ubi.img -m 2048 -p 128KiB -s 512 ubinize.cfg
my ubinize.cfg is
[ubifs]
mode=ubi
image=ubifs.img
vol_id=0
vol_size=200MiB
vol_type=dynamic
vol_name=rootfs
vol_flags=autoresize
3. in u-boot command, setenv,
#setenv nandargs 'setenv bootargs console=${console} omap_vout.vid1_static_vrfb_alloc=y rw ubi.mtd=4 rootfstype=ubifs root=ubi0:rootfs init=/init'
4. Console Logs:
UBIFS error (pid 1): ubifs_check_node: bad CRC: calculated 0xdfca80ed, read 0x7b7c0f6b
UBIFS error (pid 1): ubifs_check_node: bad node at LEB 0:0
UBIFS error (pid 1): ubifs_read_node: expected node type 6
VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 512 mtdblock0 (driver?)
1f01 1792 mtdblock1 (driver?)
1f02 256 mtdblock2 (driver?)
1f03 5120 mtdblock3 (driver?)
1f04 516608 mtdblock4 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
android_usb gadget: high speed config #1: android
adb_function_set_alt: maxsize = 512
Have anybody met the problem before?
Kernel log is attached.
Thanks,
Kevin