This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REG: Capture Test application in new released WinCE BSP(Patch 01)

There is an issue with the Video (Capture Test application) in the new released WinCE BSP. Video is not displayed when                                                                                              Capturetest /vin av /venc none /pv /auto      command is used. 

This is similar to the issue which was in previous release but it was solved when VRFB driver was disabled. But in the new release this doesnt solve the problem. 

Note :  VRFB driver and ISP Resizer are disabled.