Hi experts
1. Is it feasible to use the second MMC interface (MMC2) of TI's AM6254x as the boot of the SD card? Because this group of SDCD&SDWP and other data lines are together and can be configured.
2. Based on the speed limit of DDR4, please help measure the speed of DDR4 (relevant benchmark operation, boot time/download speed of the overall system, how to evaluate the impact of DDR4 on the overall performance? )
3. Regarding the memory size occupied by TI's sample system when running, please provide the corresponding data;
4. Please confirm whether SD_CD/SD_WP of SDIO (MMC1) can be locked to 1V8 risk;
5. If the pin level has floating voltage before the MCU is started, will it affect the power-on of the MCU?
BR
Ethan