Part Number: TDA4VM
HI expert,
I used Vision apps ETHFW to create a program that continuously sends 1460 bytes of data from the MCU20.
When I connected the cable to GESI Board PORT3 and sent the data,
On the receiving side (PC), UDP CHECKSUM INCORRECT occurs for almost all packets.
After that, when I connected the cable to GESI Board PORT4 and transmitted 1460 Byte data in the same way,
The frequency of UDP CHECKSUM INCORRECT has been improved.
(1) Why does MAC PORT3 and MAC PORT4 behave differently?
(2) UDP CHECKSUM INCORRECT may occur even if I use MAC PORT4.
Do you have any ideas for improvement?
[Connect to MAC PORT3]

[Connect to MAC PORT4]