Part Number: AM6411
Hi,
My customer is designing their own PCB board with AM64x and they have a question about AM64x with Ethernet PHY and clock. Could you please answer their question below.
On the AM64x GP EVM, the clock is input to the AM64x and Ethernet PHY via the clock buffer.
Is it needed to input the clock by synchronizing between AM64x and Ethernet PHY ?
If synchronization is not needed, remove the clock buffer from Proposal 1 of the Attachment and
I would like to have a configuration in which clocks are input to each as in Proposal 2.
If it is not required, they want to remove the clock buffer from the Case 1 and want to apply Case 2.
Is this no problem ?

Thanks and regards,
Hideaki