Dear TI teams and other engineers.
Hello, I am naru. I am trying to use UART2 in SK-TDA4VM Edge board,
but my skill (Yocto, Kernel, engineering...) is too low...
How can I add UART2 at SK-TDA4VM yocto ?
I am trying to change dts file, and check cat /proc/tty/driver/serial at board.
===========
ex:
&main_pmx0 {
myuart2_pins_default: myuart2_pins_default {
pinctrl-single,pins = <
J721E_IOPAD(0x148, PIN_INPUT, 14) /* (AA26) PRG0_PRU1_GPO18.UART2_RXD */
J721E_IOPAD(0x11c, PIN_OUTPUT, 14) /* (AA24) PRG0_PRU1_GPO7.UART2_TXD */
J721E_IOPAD(0x13c, PIN_OUTPUT, 14) /* (AF29) PRG0_PRU1_GPO15.UART2_RTSn */
>;
};
};
============
but, my message is
root@tda4vm-sk:/opt/edge_ai_apps# cat /proc/tty/driver/serial
serinfo:1.0 driver revision:
0: uart:unknown port:00000000 irq:0
1: uart:8250 mmio:0x40A00000 irq:15 tx:0 rx:0 DSR
2: uart:8250 mmio:0x02800000 irq:27 tx:38163 rx:49 RTS|CTS|DTR
3: uart:8250 mmio:0x02810000 irq:28 tx:403 rx:0 RTS|DTR|DSR
4: uart:unknown port:00000000 irq:0
5: uart:unknown port:00000000 irq:0
6: uart:8250 mmio:0x02840000 irq:29 tx:0 rx:0 DSR
7: uart:unknown port:00000000 irq:0
8: uart:unknown port:00000000 irq:0
9: uart:unknown port:00000000 irq:0
===================
I could not add UART2 (0x02820000 ?)...
please help me to set up UART 2 at SK-Edge board.
Thank you for read my question, and May the healthy be with you .