This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linking Problems.



Hi,

This question is not specific to the OMAP. It is more of a C question

I am trying to link a few compiled object files into an ELF. These are the steps I am following 

arm-none-eabi-gcc -S printf.c -o kprintf.s -I .
arm-none-eabi-gcc -S main.c -o main.s -I .

arm-none-eabi-as -mlittle-endian -o kprintf.o kprintf.s 
arm-none-eabi-as -mlittle-endian -o main.o main.s
 
arm-none-eabi-ld -Ttext 0x80008000 -entry start_armboot --start-group main.o kprintf.o --end-group -L /usr/local/gcc-arm/lib/gcc/arm-none-eabi/4.5.2/ -o u-boot 
and receive an error
kprintf.o: In function `number':
printf.c:(.text+0x3c8): undefined reference to `__aeabi_uidivmod'
printf.c:(.text+0x3e4): undefined reference to `__aeabi_uidiv'
Looking into the map of the xloader, I believe that the routines come from libgcc.a
 .text          0x0000000040205528      0x114 /usr/local/gcc-arm/lib/gcc/arm-none-eabi/4.5.2/libgcc.a(_udivsi3.o)
                0x0000000040205528                __udivsi3
                0x0000000040205528                __aeabi_uidiv
                0x000000004020561c                __aeabi_uidivmod
 .text          0x000000004020563c      0x148 /usr/local/gcc-arm/lib/gcc/arm-none-eabi/4.5.2/libgcc.a(_divsi3.o)
                0x000000004020563c                __aeabi_idiv
                0x000000004020563c                __divsi3
                0x0000000040205764                __aeabi_idivmod
 .text          0x0000000040205784        0x4 /usr/local/gcc-arm/lib/gcc/arm-none-eabi/4.5.2/libgcc.a(_dvmd_tls.o)
                0x0000000040205784                __aeabi_ldiv0
                0x0000000040205784                __aeabi_idiv0
What could I be doing wrong?
Thank you.