This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4VM

Part Number: TDA4VM

Hello, please confirm the following questions:

1.The clock of TDA4VM PCIE should generated by TDA4 internal or external clock generator? Which is better? Could TDA4 provide clock for other PCIE devices through Pin_PCIE_REFCLK if TDA4VM is available to generate PCIE clock?
2.Could you kindly review the below circuit of TDA4 PCIE?
3.Refer to below circuit, TDA4 SerDes0 connect to SWITCH while QSGMII used in TDA4, 5GBASE-R used in SWITCH, is that correct?
4.Could you please share the EMMC list which TDA4 support.
5.Could you please confirm the clock source of TDA4VM pcie0 pcie1 pcie2 is the same?
6.Should TDA4 MAIN RGMII powered by 1.8V or 3.3V, which is better,
 If TDA4VM MAIN RGMII used for 1000MHz ETH.