Dear TI/Forum members
Hardware: OMAP 3503
Software : Linux Kernel (from TI PSP linux-02.01.03.11 ) v2.6.29
Ethernet : LAN 9220 SMSC
Problem : Occasionally when we try to restart the eth0 interface when changing the IPv4 configuration, we run into two issues
Issue 1: The "Spurious irq 95: 0xffffffdf, please flush posted write for irq 37" is logged by kernel (seen via dmesg command) , this message is seen a 2 to 5 times , and no more
Issue 2: The kernel thread "softirq" consuming a very high percentage of CPU, 95% , and any operation on the system becomes very very slow , the only way to recover from this issue is to hard reboot system.
Has anyone of you face these two issues, any pointers to resolve these issue would be great
thanks
Pads