Part Number: OMAP-L138
Other Parts Discussed in Thread: ADS8557,
Following is stated on Page 876 of SPRUH77C–April 2013–Revised September 2016
"The EMIFA may be required to issue additional read operations to a device with a small data bus width in order to
complete an entire word access. In this case, the EMIFA immediately re-enters the setup period to begin another
operation without incurring the turnaround cycle delay"
What is required for additional read operations ?
When I tried to read 6 datas(16 bits) from A/D converter TI ADS8557, OMAP-L138 had six separated read operations.
- Bus width of EMAIF is 16 bits. Read address is the same at each reads, because continuous acsess is required at AD8557 six read operations
Best, Regards