Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC110: TwinCAT master gets Device Id

Part Number: AMIC110

Hi,

SDK:PRU-ICSS-EtherCAT_Slave_01.00.08.01

ECAT Master : TwinCAT3.1

Customer uses SSC 5.12 to generate a protocol stack that supports EXPLICIT_DEVICE_ID, ESI XML file, ESI EEPROM file.

The XML file that supports DEVICE_ID has an extra sentence [ <IdentificationReg134>true</IdentificationReg134>] compared to the XML file that does not support DEVICE_ID. But can't find a place to display DeviceID in TwinCAT.

A breakpoint is added at the location where the protocol stack obtains the DeviceID, and this breakpoint has not been executed after the master station is connected.