Part Number: AMIC110
We are successfully using a Lauterbach with JTAG to debug on the AMIC110 MCU on our platform.
What we would like to use is the ETM of the AMIC110 with our LA7690 PowerTrace-ETH-512M.
Our question is which lines are required from this MCU to get the PowerTrace working?
I assume that EMU 0..4 are the lines that may be used. Unfortunately we only have EMU0, EMU1 and EMU4 available. EMU2 and EMU3 are (pin)configured to be used with the MMI of a connected PHY.
We would like to know if EMU0, EMU1 and EMU4 are sufficient to get the Trace functioning?
Can these lines be configured?
Thanks for your help.