This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: How to add enet_lwip_example in mcu1.0

Part Number: TDA4VM


Hi TI Team,

I want to run the enet_lwip_example alongside with main R5f 0_0(mcu 2.0), So that I have to add enet_lwip_example_freertos code in mcu1.0(main.c).

PATHS:

Enet Example code path: ti-processor-sdk-rtos-j721e-evm-08_01_00_13/pdk_jacinto_08_01_00_36/packages/ti/drv/enet/examples/enet_lwip_example/main.c

mcu1.0 code path : ti-processor-sdk-rtos-j721e-evm-08_01_00_13/vision_apps/platform/j721e/rtos/mcu1_0/main.c

Could you please tell me what are the steps I have to follow.

1) how to add the example code in mcu1.0

2) how to compile the mcu1.0 after adding the example.

3) how to flash the binaries into the TDA4 board means by using JTAG or by using SD card.

NOTE:  I disabled the ethernet on linux A72 side, because of I want to run this example on mcu1.0 side instaed on linux A72.

 

Regards,

Sesha Venkata Harikrishna.