Other Parts Discussed in Thread: OMAP3530, ADS7846
Hello Sir i was able to Cross Compile DVSDK 3.00 for Devkit8000 and i was able to generate respective MLO, U-boot.bin and UImage. DVSDK is getting booted up with the following errors, i am not able to work on DSP due to the errors i am facing during boot up, but Angstron linux is working.
I have also attached the screen-shot of the errors and the boot parameters that i use while booting 



I don't understand where the error is??? Is it due to my filesystem that i am booting???
or the MLO, U-boot.bin, UImage that i generated???
I am able work on the Angstrom Linux but not on DSP. Even i tired using different file-systems which i got from DVSDK3.01, but in those cases even Linux is not getting booted it stays at the cmem.ko error only.
Thankyou,
Naveen Kumar.S