This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: TPS650250RHBR

Part Number: TMS320C6748

Hi,

Good day,

We are using the Power Ic TPS650250RHBR  for getting the Voltage  3v3, 1v8, & 1v3..

but we check the voltage at test point of vcc1v3d we getting 1.6v. (Check the R6 &R8 value are fine as mentioned in diagram).Actually we need the voltage of 1.3v

Again we change the voltage divider reistor value R6 & R8 there is no change in the voltage value 1.6v.

we check the voltage at pin 32 ( DEFDCDC3) is 0.8V. ; and we remove the current sense resistor R5 and measure the voltage we getting 1.1v.

Actually we need to change the voltage via  R6 &R8 or 1v3.

Kindly suggests the check points.

Regards

EG.Rajendhran